強化材と固体潤滑材を厳密に配合した物性の優れたポリマー。そして数千の評価試験によって寿命予測が可能なすべり軸受・ブッシュ、それがイグリデュールです。
イグスのエンジニアは、毎年100以上の樹脂コンパウンド新たに開発し、5,000以上の試験を実施しています。イグリデュールはすべて優れた一般的性質に加えて、用途や使用条件に応じた様々な特性をもっています。
アトミックの新しいツーリングスキーブーツでは、白色のイグリデュールGLW製フランジ付ブッシュ内、イグリデュールJすべり軸受が必要な可動性を確保しています。
WSSの接続部品では、自己潤滑性のある非常に堅牢なイグリデュール材質で作られたブッシュやつば付きブッシュが使用されています。
3Dプリンター: イグスの直動部品が生産をより迅速、弾力的に
今年の金賞受賞者は、内耳性難聴や高度難聴を治療するための、医師による人工内耳の鍵穴手術を支援するシステムです。
今年のマヌス銀賞受賞者は、コンクリート均し機です。
今年の銅賞は、チタン、アルミニウム、スチール、または金製の金属部品をプリントするレーザーベースの3Dプリント機です。
This turbine is used wherever power is used but no mains connection is available.
This binding is used on so-called splitboards.
This crane crab runs on a reconditioned crane girder.
This bicycle frame was developed as a bachelor thesis at Aachen University.
This machine is used to split tree trunks.
このハンドリングコンタクトモジュールは、温度試験キャビネット内の各基盤の自動電気測定のために使用されています。
This centrifugal clutch is used in 2-stroke racing machines.
このコルク抜きはワインの栓を自動で抜きます。
This wire-cutting machine cuts pipes for the oil and gas industry.
This 3D printer was constructed with almost no ready-made components.
This steering mechanism is used in a racing car.
This automatic packing station packs labels in boxes.
This robot is called “Porton Man” and tests protective clothing for the British military.
This robot checks the weld seams on pipes.
This isolator is used for the sterile packaging of syringes.
This column is used to store hoses or cables without twisting.
This racing car can be used both on a race track or as a rallye vehicle.
この装置は、乾いた舗装材の均しをサポートするものです。
この装置は、ポリスチレンのブロックから何らかの形やパーツを切り出すものです。
This washing machine is used in vehicle production.
This mobile robot is used during rescue operations following serious catastrophes such as earthquakes and bomb or gas explosions.
This stretching machine allows 50 percent of raw material to be saved with film/foil products.
幅を変えられる初めてのカタマラン。
The drive power of this Segway similar vehicle is directly transmitted to the wheels.
The cinema seat can be optimally positioned for spectators.
This motor robot allows providing audio- and video information also under conditions that are hazardous to health and dangerous to life.
This machine decorates cakes.
These robots have an excellent grip.
This chair can be used to sit older or weaker persons up again after a fall without a great deal of strength being necessary.
This monoski permits disabled or people with reduced mobility to ski.
このシステムは、公共及び個人のプールに波を作り出します。
This drilling machine is mounted on a trailer and is used to drill holes into concrete or asphalt.
This binding for skiers is lightweight and stable at the same time.
This motorcycle is usually to be found driving off the beaten track.
Lubrication-free plastic bearings for ergonomic office chair
光を追いかけ角度を変えて連続した太陽光発電
These sunscreen slats are supported by maintenance and lubricant-free igus® iglidur® J plain bearings.
Clean, durable, and maintenance-free: polymer plain bearings in the food industry.
iglidur® bushings guarantee clearance-free and low friction motions in RC model racing applications
Pivot and rotate with plastic plain bearings - lubricant-free designer furniture with iglidur®
頑丈な路面清掃車向けメンテナンスフリー樹脂すべり軸受
樹木移植機械は庭師や造園業者が木の植樹をするのに欠かせないツールです。
In this case, the use of igus® products is not only advantageous from a technical, but also from a financial point of view when compared to competitive products.
世界的に知られる工業用ブラシ製造機メーカーは、イグスのすべり軸受を使用しています。
Plastic plain bearings in process engineering: Completely maintenance and lubricant-free.
Due to their low weight, iglidur® Q plain bearings were used in place of bronze bushings for the spring suspension of the racing car.
フルサスペンションのマウンテンバイクで使われるイグリデュールすべり軸受
大型ヨットに仕様されているヒンジ : 完全メンテナンスフリー
海水及び摩耗に対する耐性を備えたポリマー製ベアリングが、自社製ローラーベアリングの代わりに製造現場で使われています。
非常に優れた耐摩耗性と無潤滑の特性を持つため、 イグリデュール X6 製ベアリングはワッフル焼き器に使用されています。
カーボンとアルミを材質とした、Golfcraft社のゴルフトロリー
階段はもはや、この車椅子にとっての障害ではありません。
ドライバーはこの電動自転車に、進行方向に頭を向けて、うでを伸ばした姿勢で寝そべります。
このカートレイラーでは、これまで使用してたリン青銅ベアリングをイグリデュールZ製のイグスのフランジベアリングで置き換えています。
イグスのベアリングがギアーの接続部分に使用されています。
イグスの樹脂製ベアリングが、掘削機のシートのショックアブソーバに使用されています。
湿気や究極の温度下では部品が期待値以上に拡張してしまうことがあります。
食品衛生法に準拠した高温耐性のイグリデュールA500を使ったベアリングが使用されています。
この機械は手紙を折るのに使われます。 折り込む動作には広いスペースを必要としないため、装置の枠組みサイズも小さくて済みます。
この機械は人の介入を必要とすることなく、まったく自動で書籍を読み込みます。
食品衛生上適した部品が必要となるため、設計士はクシロスボールベアリングを選びました。
これは実物の11分の1の縮尺で作られた完全な蒸気機関車です。
マシニングでは多くのチップや木くずが発生し、潤滑油に付着します。
この設計は当初クリアランスと摩擦の問題に対応するために用いられました。 しかし、イグリデュールGベアリングで、これらの問題はを解決しました。
小さな設置空間向けの耐薬品性ベアリングはイグリデュール丸棒製です。
できるだけ小さな力で動かすために、コンポーネントの軽量化が課題でした。
前輪及び後輪の駆動にイグスのすべりベアリングが使用されています。 このおかげで摩耗や腐食の問題もありません。
この電動車椅子もまた、イグスのベアリングの特性を利用しています。
この自転車用ペダルは、人間工学的及び生物学的に見た使用者のニーズを満たします。
イグスの樹脂ベアリングで、従来のローラーベアリングを置き換え、粉じんや腐食といった環境影響に対応しました。
マヌス(manus®) 2011銀賞: 芝刈機- 回転鋸(PRODULEX UNIPESSOAL LDA社、ポルトガル)
この弁は、果肉を含むアイスクリームの自動梱包装置で使用されています。
この小型車両は、磁石タイヤで表面にしっかりとくっいて、溶接ジョイントを調査します。
優れたオフロード車椅子「Quadrix」がmanus®(マヌス)コンテストにエントリーされました。
この油圧式人工膝関節では、これまで使用されていたPTFEガイドバンドをイグリデュールJのピストンリングで置き換えました。
この装置はどんなタイプの穀物でも選別し、仕分けします。 まず、空圧で対象の穀物を他のものから選別します。
このネジ転造やネジ切り修理用ハンドツールでは、ベアリングによるプロファイルローラのサポートが特に重要です。
このmanus®エントリー事例では、低価格オートメーションを使用した手作業組立での、生産でのコスト低減と加工信頼性の向上に着目しました。
イグリデュールJ丸棒から加工したベアリングは、耐食性があり低摩耗です。
一風変わった魚とり-この銛を使うと、水中で魚を捕ることができます。
この高圧洗浄機には遊星ギアボックスが使用されています。
この機械は、ブリスターフィルムで製品を包装するのに使用されています。
既存の材質を用いた新しい使用事例:この自転車のフレームは全て木製となっています。
ここでは、蜂の巣から蜂蜜を取り外します. このため、この蜂の巣は、
このソーラーシステムは単体使用だけでなく、風力発電機にも取り付けることができます。
この案内板は年中、天候や自然の猛威にさらされます。
この調査ロボットは、パイプライン専用に開発されました。
イグリデュールW300ベアリングを使用し、信頼性を向上。以前使用していたボールベアリングで必要だった定期的な給油は、イグリデュールベアリングには不要です。
使用温度が摂氏数百度に及ぶため、パイロットは防火及び耐火服を身に付けなければなりません。これに使用されているもまた、高温及び高い圧力に耐性を持っています。
これは、今回のmanus®(マヌス)コンテストのために新たに開発されたもう1台のカメラ台車です。
この折りたたみ式トレイラー「Tyligo」は、とてもフレキシブルで、様々な物の移動に使用することができます。
歩行者の邪魔にならない椅子の提供-折りたたみ椅子”シッティ”が可能にします。
最高の飛行条件を得るために、すべてのコンポーネントはできる限り軽量かつ丈夫でなければなりません。
ヘッドレストの回転にはクシロスボールベアリングが使用されています。
この機械はハーブの乾燥に使用されます。
アルミのエッジングにように、様々な材質の加工プロセスには非常に強い薬品を使用する場合があります。
3段切り替えのプロセスと、可動パーツによる衝撃に関する問題点の解決が、イグスの製品採用にあたっての決めてとなりました。
レコード回転台に使用するベアリングを設計するのに重要な課題は静かで振動の少ないことです。
このラップトップホルダーは、病院ベッド用に特別に開発されました。
この歩行補助器は、骨が脆くなる病気の子供たちのために作られました。
イグス製品を使用することで、正確な位置決めが可能となりました。
このロボット車両はとても特殊な環境用に設計されています。 いつの日にか、火星で走る製品です。
この人形は海事信号のシンボルとして使用され、もともとは人形製造業者との共同企画で作られたものでした。
この機械は製本業界で使用されている高精度測定器です。
この油圧式掘削機は実物の14.5分の1で作られたものです。
模型電車愛好家はRhätische (レーティッシュ)鉄道の電車に長年親しんできました。
使用されている石の重さは最大4000kgです。 すべての使用パーツに高い負荷がかかります。
この太陽熱発電機は化石燃料を使用せず、太陽光線からのエネルギーを使用して発電するものです。
車に座って乗ることができる患者を移送する救急車両用の、新型患者リフトがmanus®(マヌス)コンテストにエントリーされました。
この事例では、金属製ボールベアリングとDUブッシュを軽量のイグリデュールフランジベアリングで置き換えました。
イグスのクシロスボールベアリングは風力タービンのギアボックスで使用されています。
この継手は人工関節用に新開発されました。 イグリデュールJ ベアリング及びイグボール球面ベアリングが使用されています。
この機械はボックスを自動倉庫に搬入・搬出するのに使用されています。
このレーシングカーのサスペンションピンは、これまで、ベアリングを使用せず取り付けられていました。
レーシングバイクのブレーキ製造においては、超軽量であることが最大の課題です。
ドリルを使用できるほど丈夫なロボットアームです。
このグリッパーは柔軟性にすぐれています。
マヌス(manus®) 2011特別賞: ロボットヘッド(Archimedes Solutions GmbH、ドイツ)
ここでは、サラミのスライスに使用されています。 食品に触れる機械である為、大量の潤滑油を使用することはできません。
バスルームにトイレを取り付ける際イグスの製品が使用されています。
この機械は、パイル地ハンドタオルの織りとプリントを行います。
この機械は生ハムといったような加工食品にも使用されます。
使用されたすべてのイグス製品はメンテナンス不要で、機械のサービス寿命を延ばします。
「ConCut」はお菓子のCNC制御切断機です。
まず、車の上にそっとかけられたターポリンによって、車のシルエットを見せます。その後、特殊技術によってターポリンがカットされ、車が出現するのです。
このカッティング用機械装置は飲料業界で使用されています。 ここでは、複数のイグス製品が採用されています。
子供は自動ドアに指を挟みやすいものです。 このドアは”与える”ことで、それを防ぎます。
この革新的なそりでは、座ったままスキーをすることができます。 このそりは足で操縦し、手で傾けます。
この優れたスポーツ道具では、自転車に乗っているようにスキースロープを下ることができます。
この装置は、スキージャンパーのジャンプの改良に役立ちます。
イグリデュールベアリングとスラストワッシャーが芸術に一躍かっています。
このソーラーシステムは単体使用だけでなく、風力発電機にも取り付けることができます。
ソーラーシステムがその性能を発揮するには、定期的なクリーニングが必要です。砂の多い地方では、とくに重要な課題となっています。
以前は、金属のベアリング・直動ガイドを使用。すぐに錆びてしまい、頻繁なメンテナンスが必要でした。
太陽がどれほど照り付けていても建物内に差し込む光は常に快適にすることができます。
この特殊車椅子を使えば、歩行困難な人もビーチに行くことができます。
このモーターは深海6000メートルの海中で作業をします。
スペイン風オムレツ焼き機 - manus®(マヌス) 2011 金賞
この機械は食品業界で使用されています。 焼きたての製品がベルト上に配置されます。
このペダルボートでは、駆動機構の可動パーツは、スクリューが水中にあるため、無潤滑運転が求められます。
このドライトイレに使用される部品には特殊な要件が求められました。
この事例では、多重トランスミッションのボールベアリングとニードルベアリングを、イグリデュールZ製のベアリングで置き換えました。
海水は高濃度の塩分を含むため、きわめて腐食性の強い環境といえます。 海水にさらされる部品は、腐食耐性を備えていなければなりません。
ページめくり機は、障害のある人でも新聞・雑誌、ファイル、テキストなどのページを楽にめくることができるよう開発されました。
これは、三輪バイクのサスペンションの代替キットです。
新設計に、イグス(igus®)のスラストワッシャーとフランジ型ベアリングを使用。 それにより、底板のフライス加工が不要になりました。
この装置は各種製品を、さまざまな材料で梱包することができます。
この椅子は肘掛部分が調整可能で、それぞれのユーザーに合わせることができます。
これは風力を使って発電する装置です。
このエクササイズ装置は、振動で筋肉を作ります。
すべての動作が無潤滑、摩耗なしである必要がありました。摩耗があるとしても、化学分析の結果に影響しうる重金属なども出してはいけません。
イグリデュールベアリングを使用することで機械の耐用年数を4倍に延ばしました。 また、約300機械時間と約8トンの原綿を節約することができました。
以前はスチール製の部品が使用されていた、自動ネジ切り機のネジのグリッパー金具に。
鉄鋼構造、造船、ケーブルカー、プラントエンジニアリングや機械エンジニアリングに新たな可能性を与える事例です。
このスノーボード「Twistboard」は両方のパーツを軸方向に並んだジョイントでつないでいます。
オートマティック溶接プラントで使用の樹脂製ベアリング
「ケミカル・アクシデント・ロボット」の試作品は、4人の学生が制作しました。
航空機システム全体に、錆と落雷に強く絶縁性のある樹脂製ベアリングを使用しました。
この奇抜なデザインのリカンベント自転車が注目を集めています:この自転車の駆動はコードレスの揺動運動によるものです。
軽量、錆びない、低コストの ベアリング、それがこの使用の前提条件です。
農業用車両の軸ベアリングでは、局部荷重がしばしばベアリング採用の決定的条件となっています。
ケルン・ライン専門大学 : ボールグリッパーがカメラアーム伸張時の摩擦を削減
In contrast to metal and bronze bearings, the igus® bearings do not corrode due to their high-performance polymer structure and are for this reason the ideal choice for underwater application.
薬品耐性に優れ腐食しない: メンテナンスフリー ポリマー製ベアリング 、大型調理機器に使用
省スペースで腐食しないイグリデュールJ製ベアリングが、このモデルへの採用の決定打に
風、砂、太陽: 樹脂製ベアリング 、ソーラー技術に使用
短いストロークと変化する旋回角度、そして一律ではない局部荷重、イグリデュールG製ベアリング
イグリデュールG製ベアリングはメンテナンスフリーで、無潤滑運転が可能。高負荷環境での耐摩耗性と媒体耐性に優れています。
メンテナンスフリー ガイドとスライド、 透析用スツールのアーム・フットレストに使用
The plain bearings run without lubrication and without significant wear and tear
in the very harsh environmental conditions of construction machinery.
種子と直接、接触するため、完全に無潤滑で汚れに強いことが特に重要です。
国際ロボットコンテスト: ケムニッツ工科大学がライバルを探す。
摩擦と摩耗に強いベアリング、包装産業で使用
樹脂製ベアリングが無酸素に近い大気圏 で: 熱気球の飛行高度の世界記録
樹脂製ベアリングで旋回と回転 - 新しいガラス層板システム/ 「可動」外壁、自動車メーカーのサービスセンターに
伝統的なオルガン製造における、ポリマー製ベアリングの使用が増加しています。
ファーストクラスのフライ機 - 潤滑材不要の樹脂製ベアリング 、フライ用油フィルター機で活躍。食品の質を維持。
イグリデュール(iglidur®)Q製ベアリングはさまざまな旋回角度、高荷重に対応するため、電動式キックボード「ツォーブ」に最適です。
いつも稼動 - ... そして低コスト、長期的に見てシステムのダウンタイムを大幅低減。
過酷な環境下で旋回、回転。高性能ポリマー製合板機。
The rear derailleur for high-tech mountain bikes benefits from plastic plain bearings, maintenance is no longer required for MTBs.
使う人の安心を最優先 - 樹脂製ベアリングが人工関節を改善
樹脂製ベアリングがPETボトルの充填に。経済的ソリューション。
樹脂製ベアリングが、デッケルマホ・ギルデマイスター社の工作機械の製造設備で使用されています。
精密で長寿命 - ポリマー製ベアリング、新タイプの皮革分割機に
さらに長寿命 : 印刷機械に使用する特殊ベアリングの低コスト角度センサー
高いニーズを受けて この無潤滑ベアリングは衛生面で厳しい規制を受ける食品業界での使用にお奨めです。
摩耗コントロール - ベアリングと同様、とくに空圧シール検査で活用
公差調整の特殊部品、厳しい農業機械製造で
フィットネス器具の新しいソリューション、コストと組立時間を削減
優れた耐薬品性が決め手となり、イグリデュール(iglidur®)製ベアリングが採用されました。
建設機械の油圧式シリンダーにイグリデュールG ベアリング使用
イグス「ハリウッドに進出」 - ポリマー製ベアリングがカメラ設計に
超軽量。イグリデュールW300製ベアリングが、レーシングスポーツに大きなメリットを提供。
エコフロー・ポンプには、様々な大きさの「イグリデュールX」ベアリング が使用されています。
完璧にメンテナンスフリーで潤滑材不要である以外に、この使用では局部荷重への耐性が重要な意味を持ちます。
モーターで動くLEDパネルにiglidur®JVFM-0810-08(イグリデュールJVFM-0810-08)が使用されています。
汚れが堆積する環境においても、完全メンテナンスフリーのイグリデュールJ 製りベアリングが対応。
イグスのベアリングを使用することで、柔軟な動きを損なわず、ロボット下部の安定性が向上。
イグリデュールG製ベアリングは、高い摩耗耐性と完全な無潤滑運転で、この包装機械摩き布工程で性能発揮。
高い薬品耐性に加え、イグリデュールJ製ベアリングはこの使用でメンテナンスフリーの無潤滑運転を可能にしました。
高い薬品耐性に加え、イグリデュールJ製ベアリングはこの使用でメンテナンスフリーの無潤滑運転を可能にしました。
この設備では、イグリデュールJ 製ベアリングが、潤滑油を必要とするボールベアリングの代替となりました。
イグリデュールRNベアリングの使用で、 ボトル洗浄設備に必要な駆動エネルギーが大きく削減されました。
非常に優れた薬品耐性が、ピスター社のほぼ全ボトル・フランジボールにイグリデュールX製ベアリングが採用されるのに決定的でした。
連続運転では、筒型包装機械の加熱工程は時に160 °C を超えます。
メンテナンスフリーのポリマー製ベアリングを、腐食の発生しないロールチェーンに使用。主要および補助ユニットの駆動部に使用。
とりわけ、偏荷重が高かったことが、イグリデュール G プラスチック製スラストワッシャーを使用した主な目的です・。
正確且つスピーディーに矯正:これこそ正に、板金加工用機器に要求される性能をすべて満たしてるといえるでしょう。洗練された矯正加工技術により、お客様の可能性が広がります。
イグリデュールが、リキシャのさまざまな改善に
Six Flags Theme ParkのジェットコースターにイグリデュールZベアリングが使用され、大幅なコストカットが実現しました。
腐食しないことが、イグリデュールG製ベアリングを船舶用接続パーツに使用する際に重要なポイントでした。
高い摩耗耐性とメンテナンスフリーであることが、イグリデュール製ベアリング使用の決定的要因となりました。
樹脂製ベアリングを使ってのみ、潤滑油を使わないモータの使用が可能です。
潤滑材不要で腐食しない。イグリデュールGの使用が最適。
無潤滑で静か: イグリデュールG性ベアリングが診察ベッドに採用
標準の金属ロールブッシュに比べ、コスト面で大幅カットが見込まれることと、及び非常に優れた摩耗耐性を持つことが、イグリデュールD(iglidur®)材質の大きな特長といえます。
必ず当たるダーツ盤 – ミュンヘン工科大学の若いエンジニアが使用した樹脂製ベアリング
逆止め弁を統合した、段階式でシングルフローの水中モータポンプ。
イグリデュールRN製ベアリング採用により、ボトル洗浄機の駆動出力を半減することが可能となりました。
独ブルグドルフ・レールテ職業専門学校: 既存ロボットの駆動システムを、歯車駆動からベルト駆動に変換する
潤滑材がいらない 耐摩耗性ポリマー、過酷な条件の使用に - プロファイル包装機械
タイヤに載った「タマゴ」- ロッドエンドベアリングと樹脂製ベアリングが、水素駆動車を稼動。
汚れに強くメンテナンスフリー: 頑丈なロットエンドベアリングと球面ベアリング、多機能性の特殊車両に。
樹脂製ベアリング、中子造型機に使用
マヌス銅賞2007: 粉粒体ハンドリング
マヌス金賞 2007: 分割機 「オートスプリットD3」
2007年manus®銀賞: 「ボディ・スパイダー」コーペラ社
メンテナンスフリーで走行が安定
大重量も持ち上げる
高コストの修理費が発生しない
風があっても振動が少ない
食品分野だから潤滑材不要
負荷耐性が高く、TÜV検査済み
精密で人間工学を考慮
風、天候条件に強い
高温で迅速
確実なガイド
高荷重でも頑丈
長寿命で低コスト
高負荷に強い
厳しい周辺環境と汚れ
シリコン粒子が使用されるため、無潤滑運転が求められます。
ここで使用されているベアリングは摩擦抵抗が低く、頻繁なメンテナンス不要、無潤滑という特性を持ちます。
迅速で軽量
作業員1人でらくらく取付け
軽い動き
メンテナンスフリーで調合
確実で低価格
シンプルで高い耐性: 紫外線照射で効果的な硬化作用
軽量ですき間がない
静粛でメンテナンスフリー
頑丈で減振性が高い
精密で効果的
コスト削減でさらに改善
To victory with igus® - maintenance of the suspension fork eliminated.
少ない摩耗
高温と低温での使用
塩水中でも腐食しない
低価格で長寿命
摩耗耐性が高く確実
頑丈で軽量
高荷重に耐えて確実
頑丈で減振性が高い
リーズナブルでメンテナンスフリー
高温でも高い経済性
シンプルで頑丈
高い位置精度
低摩擦で静音
メンテナンスフリーで高負荷
軽量で高い信頼
確実で長寿命
17万ユーロを超える経済効果が、ポリマー製ベアリングの使用で達成されました。
高荷重でも確実: メンテナンスフリーのイグリデュールZ製ベアリングが、極度に高い負荷も吸収
印刷機械に特殊ベアリング搭載の低コスト角度センサー
従来のソリューションでは、洗浄でベアリング内の潤滑材が洗われてしまったり、ベアリング内に汚れ分子が入り込んでしまったりという問題が生じていました。
新しいメカニズムでは、従来のボールベアリングがイグリデュール樹脂製ベアリングに置き代わりました。
イグスベアリングの強みが多く活かされている使用事例として、繊維を使用したハニカムサンドイッチ構造の
飛行機が挙げられます。
このオフィス用チェアは、自動的に座る人の体重に合わせます。
グリッパーのアプリケーションヘッド
ミニショベルカー回転ローラーにイグリデュール(iglidur®)を使用し、製品寿命、可用性、安定性、荷重容量を改善
イグリデュール樹脂製ベアリング30個以上が、この使用の実現を図っています。
スクーターのステアリングは、イグスのポリマー製すべり軸受で新規に設計されました。
ハイテク飲料充填装置で使用されるベアリングの材質には、無潤滑で摩擦係数が低く、高い薬品耐性があり吸湿率が高いといった特長を持つものが適しています。
障害者の作業所に、高さ調整が可能な作業台
設計時の問題は、狭い空間のなかで2つの動きを組合せること、そして高い機械的特性が求められることでした。
ここに、イグリデュール ポリマー製ロータリーテーブルベアリングが、その軽量性により使用 。
設計者を困らせているのは、車体の重さと、それにより引き起こされる様々な問題です。そこで軽量化が実現しました。
ベアリング使用でも組立が簡単
このプリセット装置では、イグリデュールJ200材質からなるドライリンのキャリッジが、測定器としての役割を果たします。精密さを誇るこの装置は、 +/- 0.1 mmの正確性を実現します。
合板
機ACRスピードスター:ポリマー製ベアリングで低コスト
イグリデュール(iglidur®)Gは、この回転ヘッドの問題点を解決してくれます。この、回転刃は1分間に約400回転し、そのため最大30°のぐらつきが生じます。
バイオガス設備で液体性媒体の攪拌機械に使用
マウンテンバイク変速機の制御装置 (オリンピック金賞 2004).
10年来変更のなかったUVビーマーを新しく設計、詳細を変更しました。 イグリデュールGは、この回転ヘッドであらゆる問題を解決します。この回転式羽根は、1分間に400回回転します。そのため、最大30度の角度で揺動運動を伴います。
ほとんど摩耗のないベアリング機能、同時に高い, 圧迫力に耐えるチェーン、市場の要求に応じて開発
イグリデュール製ベアリングの使用で、シリンダは完全にメンテナンスフリーで、重量は元の設計に比べて10%にまで削減しました。
このカルダンジョイントは、通常のユニバーサル・カルダンジョイントに対して、ねじれ力に対応するだけではありません。
メカニカルハンドには、ハンド1つに最高99個のベアリングを使用
背もたれを調節する機講には、ドライリンが使用されており、その背もたれには、イグリデュールGを用いた樹脂製すべりベアリングを使ってヘッドレストが取り付けられています。
熱及び蒸気への耐性を兼ね揃えているという理由から、イグリデュール Xがピストンロッドをガイドするスライド部の材質に使用されています。
フラップのヒンジ部とキャスターロールに、それぞれ2つのイグリデュールZ製ベアリングを採用しました。
オルガンのドライビング・ロッドは、できるだけ静かで軽く動かなければなりません。
温度220°Cまでになるフライ油脂で使用する、そして食品耐性が高いベアリングが求められていました。 既存の問題点に対するソリューション:イグリデュールA500ベアリング
設計での課題は、製品のベアリング機能が、水または他の媒体中で使用できなければならないことでした。
ベアリング製品に対する幅広い要件を満たしているため、イグスのベアリングは標準的な機械装置にも多く使用されています。
イグリデュールX製ベアリングであれば、100℃の高温環境もクリア。
ベアリングの素材の組合せを「樹脂と金属」から「樹脂と樹脂」に変更することにより、設計の自由度が広がります。
新しいヘリコプターの負荷設備は、軽量でかつ全天候条件で確実、そしてメンテナンスフリーであることが求められます。
より良質の材質で、それでも製造コストを60%削減することができます。
核となる部分に樹脂製イグリデュールRN56の個別エレメントを採用する。この新しいデザインの採用で、求められる技術仕様条件を低コストで実現しました。
義足にかかるエネルギーおよびねじれコントロール
設計で新しいのは、イグリデュール製ベアリングをピン外側に使ったことです。
イグスのベアリングの使用により、長期間使用した後も、がたつき及び摩耗が殆どみられませんでした。
機能の基本の変化および樹脂製ベアリングの使用により、新世代の操縦輪が出現。完全メンテナンスフリーで低コストです。
可変トップの自動ロック:イグスのフランジ型ベアリングの使用で、アキシャル軸でのすきまの最大値が、1.5mmから0.5mmへ縮小。
ベアリングの新しいアセンブリで、運搬車両の駆動輪が各ベアリングの回転運動を、最小の摩擦損失によって前輪を確実に最終ステーションまで導くことを可能にします。
ここで全仕様条件を満たすのに必要だったことには、スプリングベルト付樹脂製ベアリング使用で、すき間のない取付けが可能だったことです。
自家用車のホイールキャリアのハンドリングに。顧客企業でホイールキャリアは、すでに1年にわたり、問題なく毎日、稼動しています。
このベアリング使用の特性には、以下があります。最高の品質、組込みが迅速、長寿命(スイッチ稼動200万回)、そして非常に頑丈だという点です。
ベアリングが採用されて1年、製造工程で問題なく機能しています。
イグリデュール製ベアリングの使用で、ベアリングコストを削減しました。
ボールベアリングは、とくに水中で潤滑材に問題が発生します。 またステンレス鋼のガイドは、価格の点から考えられませんでした。 また衛生上の視点からみても、樹脂製が使用されます。
内径のベアリング機能に樹脂製イグリデュールP製ベアリングを使用することによって、ベアリング公差を大きく改善することができました。
タイヤコード機にポリマー製ベアリングを使用し、安定性を向上
ドライリンリニアハウジング及びイグリデュールG製ベアリングを使用することで、センターピンの汚れを防ぎ、動きもスムーズになりました。
イグスベアリングはこの使用でとくに最適です。水、汚れ、温度に対する耐性が高いだけでなく、とくにメンテナンスフリーだからです。
この使用の主要ポイントは、高度な動的精度、高剛性で軽量、そして3シフトでの高い設備効率です。
イグスは射出成形の一体パーツを提供。これをハウジングに組込み、すでに5年間にわたって機能しています。
焼結パーツの検査:潤滑材不用のリニアガイド (液体よごれ) が確実にされなければなりません。
樹脂製ベアリングを取付けた射出成形機のスウィングアーム:差し込み式の簡単な構造と調整リングの調整により、複雑なアセンブリを可能にしました。
特殊自転車のスムーズな動きと、ハンディーキャップをかかえる人々の生活の向上を導く、イグスの樹脂製ベアリング、ボールベアリングとリニアガイド
これらのゲート駆動装置には、イグスのあらゆる製品が使用されています。
CNCドリル及びフライス盤の排気バルブ
ペダル及びレバーに使用されているイグリデュールG製ベアリングの性能は、テストで立証されています。
樹脂製ベアリングの使用で、衝撃荷重にも対応。
"Mercruiser Six号"は、高速レーシングボートです。
この機械装置に使用されているベアリングは、空気中の酸にさらされています。
コンクリート用ドリル及びコンクリート切断機における、金属ベアリングの代替品
樹脂製ベアリング使用の、ボート用モーターリフト装置及びモーターブーム巻上げ装置
完全にメンテナンスフリーであること及びスティックスリップフリーであることが、オフィス仕様の椅子には必要不可欠です。
プリンターとプロッター:低い駆動エネルギーと摩擦係数
ベアリングは、170℃ - 200℃における、25 N/mm²静ラジアル荷重に耐えます。
道路走行用及びレース用自転車のクリップレスペダル
工場内での、包装済み製品の移動用オーバーヘッドコンベアは、多種多様な製品に使用されています。
以前使われていた針ベアリングは、数年に一度の定期的なメンテナンスと交換が必要とされていました。
Lubrication-free and wear-free bushings under extremely difficult conditions.
幅広い滑りのスピード: ポリマー製ベアリングで問題知らず
多孔質のブッシングに代わり、イグリデュールM250ベアリングが採用されました。
750,000回のスウィッチの入切を、スムーズに行うことが求められました。
250℃までの高温環境で、最大2000 Nの高荷重に対応可能であることが、この装置の特長です。
非常に強い化学薬品の使用を伴う、半導体製品作りにおいては、金属製のベアリングの使用では、数週間毎に交換しなければなりませんでした。 イグリデュールX製ベアリングへの置き換えで、ベアリング部分は何年も問題なく稼動し続けています。
イグリデュール® A200 フランジ型ベアリングの使用で摩耗を低減。
この機械では、様々なサイズのイグリデュールGベアリングが使用されています。
このセンサーはクレーンの動作が停止することがないよう、(複数のクレーンを同時に)監視します。
穴あけ用器具及び電動のこぎりに使用されているベアリングは、天候面から、汚損の激しい環境にさらされることとなります。また、それにかかる衝撃荷重も考慮しなければなりません。
コンデンサの案内羽根に使用のベアリング
軽量且つ高い安定性が保たれるというメリットが買われ、イグボールロッドエンドベアリングが使用されるようになりました。
イグリデュールベアリングを使用したことで、この医療器具を提供している会社は、器具の 組立て時間が10分短縮されるなど、93%の関連コスト削減に成功しました。
メンテナンスフリーの樹脂製ベアリングを使用したデュークボックス
ベアリングを使用したコンパスのバランス保持
条件:振動を伴う周辺環境で、酸及びアルカリ性のタンク内にあり、135℃の蒸気を発するスチームパイプでの使用に耐え得る。
空気中に紙の繊維が舞った為、以前使用されていた焼結金属製ベアリングはすぐに、よごれやそれらの埃を吸着してしまいました。
回転機講から伝わる振動を最小限に抑え、ベアリングユニットは、肥料等の成分及び芝や草木中の水分に耐えられるよう、優れた耐食性を備えていなければなりません。
イグリデュールベアリングが、振動部分のベアリングとして使用されています。
このローラーテーブルは、できる限り低い駆動エネルギーが条件となる際の、イグリデュールDの使用例です。
多種多様なイグリデュールGベアリングが、この多機能車椅子のジョイントの随所に使用されています。
樹脂製ベアリングを使用した車椅子用昇降タラップが、低床バスの前扉に導入されました。
以前使用されていた金属製ベアリングと比較すると、イグリデュールX製ベアリングは切断の際、刃先から出る騒音を軽減します。
医療用ホースポンプにも安全にお使いいいただけるベアリングです。
このベアリングにかかる負荷は約10 N/mm²で、サイクル数は1日で約1000になります。
以前使用していた、回転ベアリングけは摩耗による破損が生じていました。
過酷な環境下での使用に耐える:振動、ランダム力、突然の衝撃、寒冷地、雪
スノーボードのように
ここで使用されている樹脂製ベアリングは、 無潤滑であり、経年劣化や汚れの心配はいりません。樹脂製であることから、過酷な環境条件(高温、低温、高湿、低湿)に影響を受けることはありません。
使用のベアリングは全て無潤滑でなければなりませんが、同時に冷却剤や金属切粉への耐性を保持しなければなりません。
スライド運転停止機能付き自動化ケーキデコレーション装置
現行のベアリングの壁の厚みを変更せず、その内側に収まる特別なサイズのベアリングが開発されました。
このプランジャーは電磁駆動(プランジャー用コイル)式で、空気圧によってピストンとシリンダーが動作します。
この機械装置には、回転ボールベアリングの置き換えとして、イグリデュールW300ベアリングが使用されています。
この装置を使用するとベーキングパウダー類がボールの中でスムーズに混ざり、スティック状になります。 イグリデュールJは樹脂製です。その為、汚損と薬品に対する耐性を備えています。
このテレマーク式留め具は頻繁に壊れるという問題を抱えていましたが、イグリデュール樹脂製ベアリングを使用することで、丈夫でメンテナンスフリーの製品が実現しました。
ソーセージの皮を作る装置
イグリデュール 樹脂製ベアリング 、インテーク・マニホールド
イグリデュール 樹脂製ベアリング、ベルト・テンショナーに使用
イグリデュール 樹脂製ベアリング、実用車のブレーキキャリパーに使用
iglidur® polymer bearings in undercarriages
イグリデュール 樹脂製ベアリング、ドアヒンジに使用
イグリデュール樹脂製ベアリング、オープンカーのトップ開閉システムに使用
イグリデュール樹脂製ベアリング、ペダルに使用
イグリデュール 樹脂製ベアリング、車のシートに使用
イグリデュール 樹脂製ベアリング、実用車のステアリングシステムに使用
イグリデュール 樹脂製ベアリング、エンジンのスロットルに使用
イグリデュール 樹脂製ベアリングを、運転台の油圧式ダンパーのヒンジに使用
製造コストと手間を可能な限り抑えるには、同じ部品を使用することが非常に大きな意味を持ちます。 イグスのイグリデュール製ベアリングを使用することで、安定性と柔軟性の両立に成功しました。
メンテナンスフリー及び高い費用対効果と圧倒的な扱い易さが評価され、イグスのベアリングが採用されました。
多条ねじを使用したスピンドル式リニアガイド及び、イグボール球面ベアリング搭載のテーブルリフト
グリップアームの重点課題は、ストロークの動きが簡単でシンプルな作り、そして動作半径が大きいということでした。
ドライリン - 台形ねじナット、金属シート加工機械に使用
スライド部にボールの「転がり」ではなく、樹脂製部品による「滑り」を利用したしたドライリン(drylin®)リニアガイド。バリ取り機に使用。
メンテナンスフリー ポリマー製ベアリング 、可動および固定型の製材機に
ドライリン(drylin®)リニアガイドが、コンパクトで高性能なハンドリング機に使用
ドライリン樹脂製ベアリング。オフショアドリル・ライザー検査機に使用。
イグスの製品が使用されている彫版機。4年間に渡るオートメーション技術の高度教育を受けた後、最終プロジェクトで完成をみた機械作品。
ドライリン 高温対応ベアリング、ブローバッグ製造機シーリングバーのベアリングに使用。
ドライリンをシャンパンボトルに使用
充填機械に搭載の包装用機器
ドライリンTリニアガイド、及びイグリデュールPRTロータリーテーブルベアリングを使用して, プレス加工時の動き及び旋回部品の組立ても可能になりました。
Leobotロボット:欧州ロボット大会出場を目的に設計されたロボット
無潤滑 プラスチック製 ベアリングを使用して、太陽の位置に合わせて自動的にソーラーパネルの角度を変えることで、効率良く採光することができます。
このボトル充填工場のクランプ式スターホイールにポリマー製ベアリングが導入されて以来、機械の寿命は2倍になりました。
これらの竪方向に動作する成形・充填・密閉装置で、装置の寿命が尽きるまで完全メンテナンスフリーであることは、クライアントにとって非常に重要です。
Sachs Bikes(ザックスバイク)社の試みを受け継いだNorbert Staffend社は、学生向けプロジェクトで「モーター2輪車」に焦点を当てました。それにより、飾り気の無いエレガントさを持った電動スクーターが登場しました。
シェルエコマラソンはエネルギー効率を競う大規模なコンテストで、ヨーロッパ中の学生チームが参加します。
頑丈な液体肥料用タンクローリーは、バイオガス肥料の散布を低コストで行います。 このハンドルと連動している車軸の中には、無潤滑ポリマー製ベアリングは、難しい動作や周辺環境の悪条件にも左右されません。
このプロジェクトは、模型飛行機開発に関する研究の一貫です。 イグリデュールベアリングが、補助翼の接続部分に使用されています。