Student-built personal transport vehicle uses plastic bearings2013/08/19
igus® today announced iglide® self-lubricating, maintenance-free plastic bearings are being used in the design and development of a single-passenger, urban commuting vehicle. The Personal Transport Vehicle - Ground, or "PTV-G", is the brainchild of Redbud Technology LLC out of Union Grove, Ala. Its unique design uses an articulated steering geometry, which means the inclined steering pivot is positioned just behind the occupant, and as a result reacts like a high-performance, two-wheeled motorcycle.
|