Securely guide hydraulic hoses in the smallest spaces with igus E2 hydraulic chain2018/11/14
Special challenges require innovative solutions. This is particularly true for support legs on many construction machines, such as concrete pumps or mobile cranes, which are characterised by a large variety of models, not least in the components. The safe guidance of hydraulic hoses is of crucial importance here, because they need to provide the machines constantly and reliably even under high mechanical stress and strong weather conditions. Efficient protection is provided by the E2 hydraulic chain from igus. It not only protects the internal cables, but also prevents torsion and bending of the hoses through the predefined minimum bend radius. |