The first high-tensile Profinet bus cable now available from igus2018/02/07
Profinet and other bus signals are transmitted via cables with clearly defined electrical parameters in order to ensure correct data transmission rates. Due to the low levels of current required, the cross sections of these types of cables is typically very small. The cables used are delicate and offer low permissible forces, reaching their mechanical limits quickly in hanging applications, like in modern storage and retrieval systems. |