×
トライフレックスR (「R」はラウンドの意) は、第三世代の3次元動作用エナジーチェーンです。多軸の動きに追随して電力を供給するトライフレックスRは、過酷な環境における高性能6軸ロボット用に特別に開発・設計された製品です。設計上の重要な機能として、トライフレックスRを部分的に補強するファイバーロッドオプション、チェーンリンクあたり約±10°の捻回角度、ボールソケットジョイントによる強固な連結などが挙げられます。また、トライフレックスRの製品ラインアップは100以上のコンポーネントで構成されているため、大型溶接ロボットから小型パレタイザーまであらゆる要件を満たすことができます。トライフレックスRは iFデザイン賞を受賞しました。
代表的な産業分野と用途:
産業用ロボット、工作機械、6軸ハンドリング装置、コンベヤ技術、一般機械などに最適。
コボットでの使用事例
Palletising with cobots
TRE.40.058.0.B in conjunction with the UR metal clamps ensure a trouble-free energy supply on the cobot.
Palletising with cobots
Quality control tests with cobots
The cable to the 2D camera and the vacuum hose are safely guided through the TRE.40.058.0.B and attached to the cobot with the UR metal clamps.
Quality control tests with cobots
LED bulbs production with cobots
The TRE.40.058.0.B in combination with UR metal clamps ensure trouble-free cable guidance on the cobot for LED bulb production in confined spaces
LED bulbs production with cobots
トライフレックスRの使用事例一覧:
ロボット用エンドエフェクタ
大きな作業スペースの確保と同時にロボットのエンドエフェクタと機体の間の衝突を中和
ロボット用エンドエフェクタ
Palletising robot: safe 3D cable guidance triflex® with triflex energy chain
TRE.B e-chain in combination with the retraction system (TRE.RS) allow 360° rotation of axis 6
Palletising robot: safe 3D cable guidance triflex® with triflex energy chain
Remote controlled manipulator
Special solution with 2 reverse TR.RSE.50 retraction systems ensures compact installation space with maximum retraction length
Remote controlled manipulator
3D printing in XXL format
Safe cable management through TRE.B with the pneumatic retraction system (RSP)
3D printing in XXL format
Robotic systems in automotive welding and assembly lines
Multi-axis energy supply with low-profile design.
Robotic systems in automotive welding and assembly lines
Coating with Fanuc P350
The 3D movement of the TRC e-chain with the retraction system (RSE) even allows working overhead
Coating with Fanuc P350
Heavy-duty cable robot
Move up to 250 kg freely in space
Heavy-duty cable robot
Friction stir welding with Fanuc
The special welding method using a Fanuc equipped with TR.RS.60 retraction systems and the easy-to-fill TRE.60.087.0.B
Friction stir welding with Fanuc
Deburring with Yaskawa
Deburring shower trays with a fibre-rod on a Yaskawa
Deburring with Yaskawa
Cable protection
triflex® as cable protection system in corporate colour at ING Bank.
Cable protection
Robust 3D energy chains for industrial robots in injection-moulding systems
Here, a triflex energy chain protects the pneumatic cables that are attached to a robot on an injection-moulding machine
Robust 3D energy chains for industrial robots in injection-moulding systems
Four-fold load capability
Multi-dimensionally moving energy supply system for a palletising robot
Four-fold load capability
Mobile laser hardening system
Reliable 3D energy-chain for a mobile laser hardening system
Mobile laser hardening system
3D cable guidance for Schütte CNC multi-spindle automatic lathes
Great freedom of movement at more than 4.5 million cycles per year. For this task, Schütte uses triflex R 3D energy chains from the SCX series.
3D cable guidance for Schütte CNC multi-spindle automatic lathes
Multi-dimensional energy supply system for a flame cutting machine
The energy chains and cables in this flame cutting machine encounter problems such as heat, flying sparks, and extreme amounts of dirt.
Multi-dimensional energy supply system for a flame cutting machine
Multi-directional sideloader
This sideloader solves flexible logistics tasks for wooden panels.
Multi-directional sideloader
Robots in the automotive industry
Energy supply system for robots in car factory: two-thirds fewer failures
Robots in the automotive industry
Assembly robots in the automotive industry
Multidimensionally moveable energy supply systems provide the highest flexibility and the longest holding times in all complex movements, and at the same time are installation friendly.
Assembly robots in the automotive industry
クリーンルーム技術
ロボットにつながる多くのケーブル類はまとめる必要があります。ロボットの特殊な動きはケーブル類に大きな負荷を与えます。
クリーンルーム技術
Pharmaceutical industry
The task was to design a reliable handling and also update it optically according to the latest technology.
Pharmaceutical industry
Multi-axis robots
Maintenance free with cables and multi-dimensional energy chains.
Multi-axis robots
人工衛星サルベージサービス
増え続ける宇宙のゴミ、言い換えると地球の軌道に乗るという使命を終えたものや欠損部品もまた、現代の使命の脅威となっています。
人工衛星サルベージサービス
Household appliances production
Just 24 hours passed between order, delivery and installation. The entire system functions without any problem from the first day on.
Household appliances production
Photovoltaics
Dust, sand, heat and rain: energy chain for solar technology for multi-axis movements in a photovoltaic system
Photovoltaics
Project ADVOCUT
Design of a machine tool with highly integrated mechatronic milling module.
Project ADVOCUT
Safe, flexible cable guidance for KUKA articulated arm robots in aircraft construction
An Airbus subsidiary specialised in CFRP processing in aircraft construction uses triflex R and E4/4 plastic energy chains for cable guidance.
Safe, flexible cable guidance for KUKA articulated arm robots in aircraft construction
Handling system
Robotic handling system for circuit boards. Flexible energy supply system in use in clean room technology.
Handling system
Automatic screwdriver system
A faultless supply of screws is guaranteed by the bend protection of the triflex® R system.
Automatic screwdriver system
代用ロボット
このロボットの設計士にとって、超加速がおおきな課題でした。
代用ロボット
ロボットのケーブル誘導
エナジーチェーンを使用する前までは、ケーブルはケーブルタイで束ねられていました。 しばしばケーブルの絡まりをひきおこし、コークスクリュー現象を起こしました。それはケーブル中心部の裂傷を引き起こすことになります。
ロボットのケーブル誘導
Cable guide on the industrial robot
With this industrial robot, a fixed pipe between the 3rd and 6th axis was replaced with a three-dimensional triflex® R energy chain.
Cable guide on the industrial robot
Laser-welding-robot
This laser welding robot works extremely fast. Here, a very flexible and, above all, fail-safe energy supply system is required.
Laser-welding-robot
Spot welding robot in vehicle construction
The downtimes have been drastically reduced through the use of an igus® solution for this robot in automotive construction, too.
Spot welding robot in vehicle construction
自立式プラットフォーム”アンプルマン”
“アンプルマン”と名付けられたこのプラットフォームは沖で使用されています。
自立式プラットフォーム”アンプルマン”
その他、幅広い分野で採用された使用事例はこちらをご覧ください。
用途と問題から事例を検索
エナジーチェーン使用事例
ポリマー製ベアリングの使用事例一覧