Solution
After researching, the customer came across
iglidur plain bearings, which he used to make the idea of the third bed in the VW Caddy a reality.
In addition to the space the solution saved, the customer was able to create a simple, effective solution that suited his project. In addition, the space for the fold-down bed was planned in such a way that it is flush with the centre console in the driver's cab when it is lowered, darkening the front area of the Caddy
iglidur plain bearings not only cost 40% less than metallic bearings, but plastic variants are also quick to deliver and require no lubrication or maintenance.